Camuna Cavi in-house laboratory capabilities
CAMUNA CAVI Srl is a LAPP GROUP company, a leading Italian industrial cable manufacturer, certified with ISO 9001:2008, ISO 14001:2004,ISO 50001:2011, several national and international product standards having an state of art and IMQ approved in-house Laboratory.
Here you can find the list of all tests we can perform internally in Camuna Cavi and all the tests we can perform by using an external certified laboratory.
The electrical test and routine test like tensile strength and elongation before ageing, dimensional has been omitted since we must consider included in the cable price.
These tables should be used time by time when the you will requires specific type test to be conducted on the production lot.
We can supply:
- certificates from Third Party Lab. & Report
- certificates from our Internal Lab. Test and Third Party Report - short delivery time and reduced costs, same validity as the previous one
- certificates from our Internal Lab. Test & Report with Third Party Signature
- certificates from our Internal Lab. Test & Report
Note: for some test there will be a cost for cable to be added (in small sizes the quantity of cable required by IEC 60332-3-22 CAT A could reach 600 m)